Il mio contatto
Seleziona luogo

Dopo aver selezionato il codice postale e la categoria di prodotto, vi indicheremo immediatamente la persona di riferimento per la vostra zona.

Hot chips

SCARA robot

A special design of the linking element made it possible to use this triflex® R energy supply system on a SCARA robot. This robot removes and supplies from a working area; at the same time, a rotation by 270° is performed six times a minute. The special feature of this application is the hot chips produced during the machining process, which do not stick to the igus® e-chain® and therefore extremely reduce the maintenance expenditure as a result.


INDEX Werke GmbH & Co. KG, Volker Schwohl,
Esslingen, Germany

 
 
SCARA robot  
SCARA robot  
More on applied products here
More applications from different sectors
To vector award