Dopo aver selezionato il codice postale e la categoria di prodotto, vi indicheremo immediatamente la persona di riferimento per la vostra zona.
igubal® bearing elements can be used without problems even in harsh environments and are maintenance-free. They are corrosion-resistant in humid environments. The operating temperature is from -30°C to +80°C. Seals are not necessary, even in extremely contaminated conditions. This is true for fine dust as well as coarse dirt.
Every year, igus® engineers develop more than 100 new plastic compounds and conduct more than 3500 tests on maintenance-free plain bearings every year, and thus over the years has established a large database of polymers' tribological properties.
This kiteboard has to be able to cope with heavy impact as well as with humidity and soiling.
In this packing machine, the boxes are discharged at the end of the process via the ejector unit by means of a pivoting movement.
Despite high installation costs, the solution with ball bearings and shrink tubing never achieved a proper sealing. The problem could be solved thanks to igubal® flange bearings.
In this case, the use of igus® products is not only advantageous from a technical, but also from a financial point of view when compared to competitive products.
Only extensive earthbound testing can demonstrate the suitability of components for space applications.
Light-weight and mobile robot to inspect pipes on inclines and declines.
As part of a study project, igubal® variable double spherical bearings were used in a robot with parallel kinematics due to the individual pitch sizes in small quantities.
Lubrication- and maintenance-free plastic bearings provide the required functional reliability in electric wheelchairs.
In this air bearing measuring carriage, an igubal® spherical bearing is used because of its fast and smooth precisions.
Maintenance-free igubal® pedestal bearings are used in theatre seats; they are noiseless and operate reliably even at high loads.
For this reason, drylin® linear guides and igubal® KSTM pedestal bearings are used; these need no maintenance and are not affected by the aggressive asbestos either.
This gate, which can be opened and closed automatically, is used in sport stadiums and is folded like an accordion.
This gripper picks up freshly baked goods from a conveyer belt and packs them in baskets.
When the design was revised, the metal pivoting bearings used so far were replaced by igubal® KGLM pivoting bearings.
Four igubal® pivoting bearings from igus® were tested for the floating axle through the drive, and found to be suitable after several months of tests.
The use of an igubal® EFSM flange bearing has allowed the development of a maintenance-free and silent seat mechanism element.
With this system, for example, terraces can be roofed flexibly. The roof is even waterproof in the closed state.
This machine cleans and sorts all types of grain. First the grain is separated from other material by an air current.
This inspection robot was developed especially for use in pipelines.
Since temperatures of several hundred degrees Celsius occur here, the pilot must wear fire and heat-resistant clothing. The bearings used also have to withstand the high temperatures and pressures.
This adjustable camera tripod is usually used for cameras that have their centre of gravity well beyond the bearing axis.
To achieve the best flying conditions, all components must be lightweight and at the same time as durable as possible.
The special device needed to be as economical as possible in its construction, and the individual components as maintenance-free and durable as possible.
Here, igubal® plastic rod end bearings from igus® are used in the steering on an electric wheelchair.
This robotic vehicle is designed for a very special environment: it will one day be driving on Mars.
This pagepulltester is a high-precision measuring instrument for the bookbinding industry.
This joint is a new development to be used in prostheses. iglidur® J plain bearings and igubal® spherical bearings are installed in it.
Each machine contains 69 igubal® fl ange bearings, which were chosen on account of their corrosion resistance, lubricant freedom and space-saving design.
With this application, salami is cut into slices. As with all applications in contact with food, here too lubricants cannot be used.
The prototype of the „Sunseeker Duo“ solar plane is the world‘s first solar-powered two-seater.
Previously, metal bearings and linear guides were used, which rusted quickly and therefore required frequent maintenance.
The screwconveyer of the gritting unit has to be mounted movable in order to compensate axial offset and dynamic movements in the screw.
This motor is to drive deep-sea robots even at 6,000 metres under the sea.
igus® thrust washers and flange bearings were used for the new design. They made the elaborate milling of the base plate unnecessary.
the armrests of this chair are adjustable, to accommodate the needs of the individual user.
The steering unit, inclusive of the steering rod, is made of carbon fibres and is mounted with igubal® flange bearings and igubal® rod end bearings. These allow a weight reduction of about 30 per cent compared to other solutions.
Since the tank is filled with salt water, the components used may not be susceptible to corrosion.
The igubal® flange and pillow block bearings compensate for the misalignments of the bent structure on this self-propelled golf caddy.
In the accessory equipment for lawn care and outdoor cleaning, the igubal® flange bearings offer good value at a low price and a simple possibility for a corrosion-resistant bearing.
igubal® as alternative to metallic bearings in paper banding machines prevents the shaft from "seizing".
igubal® flange bearings put an end to corrosion, maintenance and expensive stainless steel alternatives in drive bearings of conveyor systems in the food sector.
Mirror adjustment of the telescope is performed virtually free of backlash with igubal® rod end bearings.
igubal® spherical bearings of the dimensional series E by their maintenance-free feature and the omission of lubricants prevent any failure through the sticking together of textile fibers.
The maintenance-free spherical bearings in the carbon yoke compensates for the frame and spring movements resulting from the dynamic quality of driving.
Lubrication-free tribopolymers in extreme application - Packaging unit for profiles.
Egg on four wheels - How rod end bearings and plastic bearings make a hydrogen-powered vehicle mobile.
The igubal® clevis joints made of plastic offer a cost-efficient alternative to stainless steel clevis joints
Corrosion-resistance and the low component weight are criteria which tipped the decision in favor of the igubal® components.
Arguments for noise minimization and reduction of maintenance rate were decisive here.
The spherical igubal® coupling between motor and camera dolly permits speeds up to 3m/s in curves.
The lifting device's own weight and thereby the rotating bulk and the load of the drive are reduced by the use of igubal® spherical bearings made of tribopolymers.
The pivoting and linear feed movement is implemented by means of drylin® linear guides and igubal® spherical bearing components.
In this two-wheeler, the linkage of rear wheel to the frame is implemented by means of maintenance-free rod end bearings.
Decorations without lubricants by using the maintenance-free igubal® rod end bearings make any sweet most relishable.
In outdoor use, the igubal® rod end bearings perform their task absolutely free of maintenance.
The rod end bearings for the steps of the caravans are tough and insensitive to dirt.
The maintenance-free igubal® rod end bearing is used as connecting component between pneumatic cylinder and adjusting lever.
No maintenance, no corrosion and the igubal® rod end bearings, painted in the housing color of the sensor, additionally form one unit with the cylinder
Concentricity errors and shocks are compensated for by means of spherical rod end bearings in the support of the thread guide unit for the thread winder.
The used igubal® spherical bearings are insensitive to media in the surroundings and are thereby absolutely maintenance-free.
igubal® spherical bearings are used in the main bearing assembly of every individual slat due to their freedom from maintenance, corrosion resistance and atmospheric resistance.
Dust-repellant and maintenance-free: The tough rod end bearings and spherical bearings do a sturdy job in the special-purpose municipal vehicles.
igubal® spherical bearings as insulating components in current consumers of the subway.
The stroke movement for a high-frequency, fully automatic enveloping system is implemented by plastic pillow block bearings and rod end bearings.
Abrasion, corrosion, high service life, resistance against cleaners were criteria for an application in the food sector.
Simple pivot movements as well as compensation of misalignments are implemented in bearing assemblies of drive shafts and chain sprocket bearings with plastic pillow block bearings.
igubal® rod end bearings are used in the titling mechanism of this recumbant bike.
It is possible to compensate alignment faults with igubal® spherical bearings.
In leaching systems and transport equipment, igubal® pillow block and flange bearings compensate for potential errors in the alignment of sheet metal equipment.
Both the housing material and the universal ball and socket connection are made of food-compatible materials.
The rod end bearings in the connection couplings withstand the fruit acid of grapes.
Long service life with concurrent food-safe design characterizes this application.
Con questo piccolo robot, Jonas Thees ha partecipato al RoboCup 2006 a Brema. Il quattordicenne ha vinto il campionato mondiale nella sezione junior per il Robot Rescue con il progetto presentato.
The used clevis joints and rod end bearings are corrosion-free and usable in liquid media.
Maintenance-free track accuracy
No lubricants in food sector
Can be handled alone
The bearings reliably transmit the high radial centering forces with low friction and free of stick-slip and minimize the arm system's friction through their integrated start-up.
The challenge: The operating temperature is maximum 140°C and the applied material must be resistant to all cleaning agents used in the beverages industry.
The objective was to keep the weight of the climbing robot as low as possible, so that it can move with suction cups on smooth surfaces like window panes.
A problem that vexed the designers was the total weight and the occurring leverages. Here the weight should be saved.
Polymer bearings in electric cars for children: Top quality was achieved.
iglidur® G is the problem solver in this rotor head The rotor blades rotate about 400 times per minute and thereby execute oscillating motion with maximum 30°.
Locking mechanism of a banknote processing machine: The double joint enables all necessary degrees of freedom and also absorbs the tensile strength.
Steering linkage of the hydrogen-powered world record vehicle HYSUN 3000.
Requirements for the design were stiffness, low-priced relocation and dirt resistance.
The igubal® ball heads are particularly well-suited for this requirement. They do not indicate any notable clearance even after about 15 million operation cycles.
A novel external load system for helicopters required a low weight, high reliability with simultaneous weather resistance and freedom from maintenance.
Kinematic system for automobiles: The employed plain bearing enables a tolerance adjustment of the loading platform to the side paneling.
Ball bearing assemblies are very precarious due to the lubricant particularly under water. Stainless steel guidances cannot be considered due to the high costs. Plastic is used also for hygienic reasons.
Application of polymer plain bearings in bagging machines for caustic soda.
The igubal® flange bearings were by far the most cost-efficient alternative in comparison.
Conventional guide systems break down as no oil or fat whatsoever should enter the dipping bath.
Plain, spherical and linear bearings made of plastic help to improve mobility and the quality of life
Basketball shooting device for wheelchairs: Due to igus® products only a little energy is lost through friction, and there is only a minimal angular shift when the shaft accelerates vertically.
Transfer of the steering movement in a "Body-Turn-Bike" by two rod end bearings.
JAM-08 pillow block bearing and KBRM-08 rod end bearing in a meat portioner / packing device
Truck-mounted customized spraying systems for gardening and tree care companies.
Due to their lower weight and better suspension qualities, the company switched to igubal® rod end bearings.
Polymer rod end bearing in a smoke extraction system at a meat factory.
The spherical bearing used compensates the angle misalignment. That means no more maintenance is necessary.
Used in difficult conditions: vibration, random forces, sudden shocks and cold, wet snow.
Application of a high-value spindle lift table with steep-threaded spindle, linear guide systems and igubal® spherical bearings.
The aim of the concept is to demonstrate to the students how to handle a programmable logic controller (abbreviation: PLC) in an attractive way.
Il robot di restauro della Hans Böckler-Schule al Berufskolleg di Münster combina tecnologia e storia dell'arte.
Maintenance-free plastic bearing defy all outer influences and provides for the required service life.
The unusual design for a recumbent bicycle has got what it takes: cordless screwdrivers are used here to drive it.
Wind, sand and sun: Plastic plain bearing for solar technology
New solutions for fitness equipment save production costs and assembly times.
Quick, straight, precise: this is how the requirements in sheet metal machining can be summarized. Sophisticated straightening technology makes all this possible.
Bearings on steering linkage and connection in a racing beer crate.
Steering/damper connection on a Formula 1 model racing car.
Reliable and vibration dampening linkage on the swashplate and the rotor guide.
On these horizontal forming, filling and sealing machines, the total freedom from maintenance over the machines' entire life cycle was particularly important for the customer.